CAN and two UARTs in 20 pin TSSOP STM32F042?
Hello, can the pin configuration shown below possible?
We need one bidirectional UART and a CAN along with a UART TX for debugging.
Questions are:
- It says "Pin pair PA11/12 can be remapped in place of pin pair PA9/10 using the SYSCFG_CFGR1 register" So I would only need PA10 to be remapped to PA12 for CAN TX. Is this possible?
- Can USART be initialized with only TX pin?
- Would there be any issue with using CAN RX with BOOT0 pin?
Thanks, Prithvi