Skip to main content
ZB.1
Associate II
December 10, 2020
Question

Error downloading Thread_SED_Coap_FreeRTOS

  • December 10, 2020
  • 3 replies
  • 2449 views

Hello there

I am using the official engineering code Thread_SED_Coap_FreeRTOS. When downloading with STM32CubeProgrammer, the error message connection to device0x495 is lost appears. At this time, the program should fail to download because the LED1, LED2, and LED3 on the board are not lit, so I want to use it again When downloading programs on this board, STM32CubeProgrammer reported an error ERROR:NO STM32 TARGET FOUND. What is causing this? I downloaded other project codes normally.THANK YOU0693W000006FJo9QAG.jpg0693W000006FJqoQAG.jpg0693W000006FJp2QAG.jpg

This topic has been closed for replies.

3 replies

ST Technical Moderator
December 11, 2020

Hello @ZB.1​ ,

Welcome to the STM32 Community :smiling_face_with_smiling_eyes:.

Which version of STM32CubeProgrammer are you using ?

I see that you are using an old version of STM32CubeWB firmware package (v1.8.0).

Please ensure to use the latest version of the STM32CubeProg tool (v2.6.0) and STM32CubeWB firmware package (V1.10.0).

If this issue is reproduced with latest release, please provide more information about your board, which may help to reproduce this behavior.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ZB.1
ZB.1Author
Associate II
December 26, 2020

I have tried the latest firmware package STM32CUBEWB V1.10.0, but it still fails。

ZB.1
ZB.1Author
Associate II
December 21, 2020

Hello, thank you very much for your answer. I am sure that I have upgraded the STM32 CubeProgrammer to the latest version, and I am using the version V1.9.0, but the problem still exists.I only found 1.9.0 STM32CubeWB on the official website.Hope to have a solution soon, thank you0693W000006GPsnQAG.jpg0693W000006GPsiQAG.jpg

Houda GHABRI
ST Employee
January 5, 2021

Hi @ZB.1​ 

Can you please try to connect with "Under Reset " Mode instead of "Normal" mode?

Houda

ZB.1
ZB.1Author
Associate II
January 5, 2021

Thank you very much for your answer. Under your suggestion, I tried again, but the problem was still not solved, and I didn’t see the effect that this project should have.0693W000006HYRiQAO.jpg