Associate
December 6, 2020
Question
Issue with ESC001V1
- December 6, 2020
- 1 reply
- 772 views
Good Evening,
I am an STM user, I used it for a lot of project and I am familiar with it.
Now I am trying to start a Drone project and I have the STEVAL-ESC001V1 Controller (Link bellow).
When I tried using the motor profiler or even the STM Workbench I couldn't choose it! Since it has to be used only with the other STM32F303CB based STEVAL-ESC001V1. (Picture bellow)
I have 2 questions.
- Can the 2nd STEVAL-ESC001V1 be used with any controller other than the 303CB in the motor profiler picture bellow ?? The STM32F303RE for example ?
- The left STEVAL-ESC001V1 is written to be not approved for resale ! So please if I want to use the 2nd STEVAL-ESC001V1, Which controller should I use with it in order to be able to use the Workbench and Motor Profiler ?
STEVAL-ESC001V1 Link:
https://www.st.com/en/evaluation-tools/steval-esc001v1.html#overview
Motor Profiler Screenshot:
Thanks a lot.