Question
Boot configuration for STM32G071
For STM32G071 controller, I see difference in information provided in Ref manual (RM0444 Rev4) and STM32 microcontroller system memory boot mode applicate note(AN2606 Rev44).
- In Ref manual on Pg 60 section 2.5 it is mentioned that for selecting boot from system memory we’ve 2 options.
- Option Byte from Ref Manual, pg no 73 section 3.4.1 says that all nBOOT0, nBOOT1, nBOOT_SEL bits are 1
- so any of the option to select system memory boot will not work unless I change the option byte value in user application or using tools like STCubeProgrammer or DFuseDemo
- In Application note(AN2606), on pg no 206 section 40.1 it is mentioned to refer pattern 11 from table 2 for STM32G07 controllers.
- Pattern 11 from table 2 pg no 24 section 4.1, 2nd option does not check nBOOT0 bit in option byte. So this option does not require any change in option byte as rest fields nBoot1 and nBOOT0_SEL bits are already set to 1 as in default value.
My questions:
- Is there error in documentation wherein this difference is just an error?
- If there is error in documentation, can I get correct document?
- If Application note(AN2606) is correct then can I enable boot from system memory?
Thanks,