How to read PDM microphone with the Serial Audio Interface(SAI)
- December 3, 2020
- 2 replies
- 1674 views
I have a really simple application setup. I'm currently feeding in one PDM microphone. I'm using the SAI interface (code is attached). First there appears to be a bug in the ST code. The SAI_PDMCR register have a field to set up to 4 microphones (see reference manual).
The STM32CubeMX doesn't allow you to set the value to anything other than a 3. If you set it to a 4, this assert will fail:
#define IS_SAI_PDM_MIC_PAIRS_NUMBER(VALUE) ((1U <= (VALUE)) && ((VALUE) <= 3U))
But the code that sets the register is shown here (line 759 of stm32h7xx_hal_sai.c)
SaiBaseAddress->PDMCR = (hsai->Init.PdmInit.ClockEnable | ((hsai->Init.PdmInit.MicPairsNbr - 1U) << SAI_PDMCR_MICNBR_Pos));
So you can never enable the 4th microphone pair. My next problem is I never receive any PDM data. I can see the clock coming out of the SAI clock pin (although the clock makes no sense from what I tried to set).
I then call :
HAL_SAI_Receive_IT(&hsai_BlockA1, audioData, 48000);
and set a breakpoint into the PDM interrupt. But the interrupt is never called. I'm at a bit of a loss. Looking at the SAI status register, the FIFO is always empty.
I'm attaching the example project.