Skip to main content
NBhat.1
Associate III
December 2, 2020
Solved

Can't run st-example-image-qt QT examples on a custom board based on STM32MP153C with RGB panel

  • December 2, 2020
  • 5 replies
  • 2416 views

I'm trying to run QT examples on a build created using st-example-image-qt (Ecosystem v2.1) on our custom board. We have a simple RGB display 800x480 resolution, so I modified the cursor.json on the board as follows

{

 "device": "/dev/dri/card0",

 "outputs": [

   { "name": "DPI1", "mode": "800x480", "size": "800x480" }

 ],

 "hwcursor": false

But when I try to run any QT example I get the following error

root@stm32mp1-midmark:/usr/share# psplash-drm-quit

root@stm32mp1-midmark:/usr/share# export QT_QPA_EGLFS_ALWAYS_SET_MODE="1"

root@stm32mp1-midmark:/usr/share# examples/opengl/hellowindow/hellowindow

[   1] Failed to open device: No such file or directory, Try again...

[   2] Failed to open device: No such file or directory, Try again...

[   3] Failed to open device: No such file or directory, Try again...

[   4] Failed to open device: No such file or directory, Try again...

[   5] _OpenDevice(1086): FATAL: Failed to open device, errno=No such file or directory.

[   6] Failed to open device: No such file or directory, Try again...

[   7] Failed to open device: No such file or directory, Try again...

[   8] Failed to open device: No such file or directory, Try again...

[   9] Failed to open device: No such file or directory, Try again...

[  10] _OpenDevice(1086): FATAL: Failed to open device, errno=No such file or directory.

root@stm32mp1-midmark:/usr/share#

What do I need to do to run QT examples on a simple RGB panel?

Thanks.

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi,

For reference for anyone interested.

Issue was due to dependances of QT with GPU ... not present on MP153.

To make it work, follow the sequence in :

https://wiki.st.com/stm32mpu/wiki/How_to_build_and_use_an_SDK_for_QT#QT_image_and_SDK_with_EGLFS

but DO NOT ACCEPT EULA !!!

Without EULA the vivante driver and the associated libraries are not built.

The "mesa" package is installed in place of vivante's stuff.

Mesa is able to deal with GPU-less devices.

The example

/usr/share/examples/opengl/hellowindow/hellowindow

works fine. Slow because fully SW emulated, but it works!

Olivier

5 replies

Olivier GALLIEN
ST Technical Moderator
December 9, 2020

Hi @NBhat.1​ ,

Same issue has already been enter by our local FAE.

We will first answer by this thread.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
December 16, 2020

Hi,

For reference for anyone interested.

Issue was due to dependances of QT with GPU ... not present on MP153.

To make it work, follow the sequence in :

https://wiki.st.com/stm32mpu/wiki/How_to_build_and_use_an_SDK_for_QT#QT_image_and_SDK_with_EGLFS

but DO NOT ACCEPT EULA !!!

Without EULA the vivante driver and the associated libraries are not built.

The "mesa" package is installed in place of vivante's stuff.

Mesa is able to deal with GPU-less devices.

The example

/usr/share/examples/opengl/hellowindow/hellowindow

works fine. Slow because fully SW emulated, but it works!

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
April 22, 2024

Would this also be relevant to the stm32mp151 as well?

danfly09
Associate
April 15, 2022

In my case it seems Qt is trying to run on /dev/fb0 which is not defined, instead of /dev/dri/card0

Any ideas?

bgate.1
Visitor II
August 9, 2022

seems that your default platform is linuxfb

QT_QPA_PLATFORM=eglfs