Skip to main content
ANiko.3
Associate II
December 2, 2020
Solved

Changing the eMMC pins with OTP

Hello,

I have a custom board based on STM32MP151-C with an eMMC on the following pins:

  • SDMMC2_CK PE3 (AF09)
  • SDMMC2_D0  PE6 (AF07)
  • SDMMC2_CMD   PG6 (AF10)

I read that the ROM expects the the SDMMC2_D0 pin on PB14 so I need to change it by using values from the OTP. I found this link (https://community.st.com/s/question/0D50X0000AkQJiHSQW/how-to-change-emmc-interface) and did the same as the ST Support, just for my pins. Here are my results.

  • OTP3 = 0x00000004    SDMMC2 (uses non default AFmux defined in OTP)
  • OTP5 = 0x38745394
    • SDMMC2_CK = PE3 (bits[15:0]: port0=5=GPIOE, pin0=3, afmux0=9, mode0=4=AF;pull-up;medium-speed)
    • SDMMC2_D0 = PC8 (bits[31:16]: port1=3=GPIOC, pin1=8, afmux1=7, mode1=4=AF;pull-up;medium-speed)
  • OTP6 = 0x000076A4
    • SDMMC2_CMD = PG6 (bits[15:0]: port2=7=GPIOG, pin2=6, afmux2=10, mode2=4=AF;pull-up;medium-speed)

Could someone please let me know if I calculated the OTP values correctly? So I dont brick the board.

PS: How do I determine the speed on the pin (low, medium or high)?

Thanks.

This topic has been closed for replies.
OlivierK
OlivierKBest answer
ST Technical Moderator
December 2, 2020

​Hi ANiko.3,

You've stated 2 different configurations for SDMMC2_D0

According to your configuration (PE3/PE6/PG6) , I found

OTP3 = 0x00000004

OTP5= 0x56745394

OTP6 correct.

or to your configuration (PE3/PC8/PG6) , I found

OTP3 = 0x00000004

OTP5= 0x38745394 (correct)

OTP6 correct.

Kind Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

10 replies

OlivierK
OlivierKBest answer
ST Technical Moderator
December 2, 2020

​Hi ANiko.3,

You've stated 2 different configurations for SDMMC2_D0

According to your configuration (PE3/PE6/PG6) , I found

OTP3 = 0x00000004

OTP5= 0x56745394

OTP6 correct.

or to your configuration (PE3/PC8/PG6) , I found

OTP3 = 0x00000004

OTP5= 0x38745394 (correct)

OTP6 correct.

Kind Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee
December 2, 2020

Hi,

note that there is no SDMMC2_D0 on PC8, so the second config will not work.

Also note that eMMC boot is working only with few memory brand if you have silicon Rev.B. Silicon Rev.Z is corrected. See ES0438 for details (this is mentioned in the post you refer, so I think you are already aware).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
ANiko.3
ANiko.3Author
Associate II
December 2, 2020

Hi to both of you and thatnks for the answer. Yes, I made a typo with the SDMMC2_D0 pin (PC8 is coming from the example), so the first configuration is the one I need.

@PatrickF​ We have the Rev.Z and the THGBMNG5D1LBAIL eMMC, so there shouldnt be a problem, but thanks for mentioning anyway.

I have a question for the Pin Mode. I set the Pin Mode to 4 which means "AF ; pull-up ; medium-speed"

  • All three pins in question have a pull-up resistor of 10k to the 3.3V. Is that meant by the pull-up in the pin mode?
  • The eMMC we have is THGBMNG5D1LBAIL. Is medium-speed the correct settings

Thanks.

PatrickF
ST Employee
December 3, 2020

With those OTP settings, we enable the internal pull-up (this is already the case with default BootROM eMMC pins). No issues to have both internal and external pull-up.

External pull-up on some eMMC signals are anyway required to avoid (slight) overconsumption from the eMMC in STANDBY (where all MP1 pins are floating as no VDDCORE), this is because usually the eMMC is still partly powered in platform Standby mode (e.g. VCCQ=VDD).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
alenik-mm
Associate II
December 3, 2020

Great, thanks. What about the speed? Is medium-speed correct?

ANiko.3
ANiko.3Author
Associate II
December 3, 2020

Hello,

I set the OTP words 3, 5 and 6, but somehow the board doesnt boot. Here are my values now when I read them out of the OTP:

03 0x00000004     0         0         0         0         0         0

05 0x56745394     0         0         0         0         0         0

06 0x000076a4     0         0         0         0         0         0

The power consumption is a bit higher than when the CPU is in the serial boot mode. The TF-A is not sending anything over UART4 though. The Boots pins should be set correctly: 010.

Any thoughts?

PatrickF
ST Employee
December 3, 2020

Hello,

is the board fall back to Serial Boot (coud be seen on PA13 toggling. note that it is open drain driven, so need an external pull-up) ?

If yes, you need to analyze the Boot trace by doing a SYSRAM dump. See https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview#Debug_and_Error_messages and https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_trace_analyzer

To dump the SYSRAM traces, without resetting the board after failure, you could use the following command on your Linux PC

openocd -f board/stm32mp15x_dk2.cfg -c 'init;cortex_a smp off;halt;dump_image traces.bin 0x2ffc1c00 2048;resume;shutdown'

Otherwise, your TF-A has been launch and you need to debug it.

Maybe see https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
alenik-mm
Associate II
December 3, 2020

Hi Patrick,

it was the TF-A device tree -I had to update it. Now I can boot up to the U-Boot successfully. Thanks again for your support.

PatrickF
ST Employee
December 3, 2020

Glad to see it is working.

Please click on 'Select as Best' if our replies solved your issue or answered your question

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent