Skip to main content
LKevi.1
Associate
November 29, 2020
Question

ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed

  • November 29, 2020
  • 3 replies
  • 2483 views

HI,all,

env:virtualbox, ubuntu18.04 64bits, 10G memory,500G disk.

I tried to build rootfs image from stm32 Yocto prject, followed by wiki(https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package).

but I got some error at last like below.

I am a newer for YOCTO, what can I do next? any idea?

Thanks a lot.

error log:

ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs

ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs.11363

ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs) failed with exit code '1'

This topic has been closed for replies.

3 replies

Christophe Guibout
ST Technical Moderator
November 30, 2020

Hi @LKevi.1​ ,

Did you have this error after executing bitbake st-image-weston ?

Could you please share the logfile of failure (log.do_rootfs.11363) ?

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LKevi.1
LKevi.1Author
Associate
November 30, 2020

Hi, Christophe Guibout:

Yes, I got this error after executing bitbake st-image-weston, like below log, and the detail log as attach

Thanks for your reply!

​

$ bitbake st-image-weston

NOTE: Started PRServer with DBfile: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 36013, PID: 21361

Loading cache: 100% |###########################################################################################| Time: 0:00:03

Loaded 3743 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

​

Build Configuration:

BB_VERSION      = "1.46.0"

BUILD_SYS      = "x86_64-linux"

NATIVELSBSTRING   = "universal"

TARGET_SYS      = "arm-ostl-linux-gnueabi"

MACHINE       = "stm32mp1"

DISTRO        = "openstlinux-weston"

DISTRO_VERSION    = "3.1-snapshot-20201130"

TUNE_FEATURES    = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"

TARGET_FPU      = "hard"

DISTRO_CODENAME   = "dunfell"

ACCEPT_EULA_stm32mp1 = "1"

GCCVERSION      = "9.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"

meta-python      

meta-oe        

meta-gnome      

meta-initramfs    

meta-multimedia    

meta-networking    

meta-webserver    

meta-filesystems   

meta-perl      = "HEAD:144077083457ccb75700777d5e6b1da9aaff01aa"

meta-st-stm32mp   = "HEAD:955b1d9a5f706013d718687b1afa6e3022c68fac"

meta-qt5       = "HEAD:fdd19517e17240b0b61765bd02fc483a1bde986f"

meta-st-openstlinux = "HEAD:9160c08dfcd0b7ec0eb8f1fd96672695b09680d5"

meta         = "HEAD:b39bda4cc62db12c0edfbe489d5a7f5988ede6a9"

​

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:14

Sstate summary: Wanted 415 Found 398 Missed 17 Current 2904 (95% match, 99% complete)

NOTE: Executing Tasks

ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs

ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs.21480

ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs) failed with exit code '1'

Waiting for 3 running tasks to finish:

ERROR: st-image-userfs-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_immodules_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-userfs/1.0-r0/temp/log.do_rootfs

ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-userfs/1.0-r0/temp/log.do_rootfs.21635

ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb:do_rootfs) failed with exit code '1'

ERROR: st-image-weston-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_immodules_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-weston/1.0-r0/temp/log.do_rootfs

ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-weston/1.0-r0/temp/log.do_rootfs.21723

ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb:do_rootfs) failed with exit code '1'

ERROR: st-image-vendorfs-1.0-r0 do_rootfs: The postinstall intercept hook 'update_font_cache' failed, details in /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-vendorfs/1.0-r0/temp/log.do_rootfs

ERROR: Logfile of failure stored in: /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-vendorfs/1.0-r0/temp/log.do_rootfs.21645

ERROR: Task (/media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb:do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 9046 tasks of which 9031 didn't need to be rerun and 4 failed.

NOTE: Writing buildhistory

NOTE: Writing buildhistory took: 20 seconds

​

Summary: 4 tasks failed:

 /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs

 /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb:do_rootfs

 /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb:do_rootfs

 /media/kevin/D2/openstlinux-5.4-dunfell-mp1-20-11-12/layers/meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb:do_rootfs

Summary: There were 4 ERROR messages shown, returning a non-zero exit code.

​

Christophe Guibout
ST Technical Moderator
December 1, 2020

HI @LKevi.1​ ,

Unfortunately, the logs don't give more information.

I would recommand to restart the compilation : bitbake st-image-weston -c cleansstate && bitbake st-image-weston

If it still doesn't work, you can cleanup a bit more : bitbake st-image-weston -c cleanall && bitbake st-image-weston

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.