Associate III
November 29, 2020
Question
How does the USART 2 transmit signal output from pins PA2 and GND to a logic analyser?
- November 29, 2020
- 2 replies
- 2966 views
I am having a little difficulty getting a USART 2 signal to output to a logic analyser using transmit Tx serial asynchronous communication. I have configured a USART 2 peripheral to communicate through a DMA. The GPIO pin PA2 is outputting a constant logic one, so I am guessing I have missed something on the STML476VG DISCO microcontroller. I have tried to set the LSE clock to 32.768 kHz to no success. I have the low power sleep mode HAL driver configured in the source code. I have tried to change the parity setting in the IDE to even, but no luck.