Skip to main content
HK_it
Associate II
November 27, 2020
Question

STM32WL QFPN package reference design and board layout ?

  • November 27, 2020
  • 4 replies
  • 3426 views

I want to make custom stm32WL board layout with antenna path. I found NUCLEO-WL55JC. This board has BGA package for stm32WL55JC.

Q1: I need stm32WL QFPN package board layout and antenna path. Is there board layout and reference design for stm32WL55CC (QFPN) ?

0693W000005CtgzQAC.png 

Q2: I see rf-shield for stm32WL55JC in NUCLEO-WL55JC board. What is ordering code of rf-shield and where can I buy this ? I shared rf-shield screenshot in attachment.

0693W000005CtfwQAC.png 

Thanks in advance.

This topic has been closed for replies.

4 replies

Remi QUINTIN
ST Technical Moderator
November 27, 2020

Regarding files describing the layout of a reference design using the stm32WL55CC, I will check if we have something ready to deliver.

Regarding the RF shield, it is the same as the one use for the STM32WB microcontroller populated on the Nucleo board. It is a « home-made » design done by a very local company (Embest). I don’t know if they can be ready to distribute it. I will ask them.

RFerr.3
Associate II
December 18, 2020

Hi @Remi QUINTIN​ , any news about the QFN reference design ?

Hamilton DC
Visitor II
January 6, 2021

Olá @RFerr.3​ ,

Attached the file for QFN Ref. Board.

The schematics with the RF BoM PDFs are under "Manufacturing\3.2. Schematic, Assy & 3D PDF\Schematic\".

Att,

Hamilton

RFerr.3
Associate II
January 16, 2021

Thanks @Hamilton DC​ 

With this example project i could manage to project a 2 pcb layer using all gpio!