Skip to main content
spark
Associate II
November 26, 2020
Question

STM32F7 Discovery kit for STM32F746 MCU

  • November 26, 2020
  • 1 reply
  • 1544 views

Hi,

I started to work with the STM32F7 Discovery kit and according to the instruction I set JP1 to 5V_STLINK and then I connected the USB cable from the kit to the PC to power the board. The outcomes are:

LD7 is red, LD2 is red and the LD4 is green. But the screen brightness is really almost dark! and really difficult to see applications lists.

Please find the attachments.

Kindly help!

0693W000005CpAaQAK.jpg0693W000005CpB4QAK.jpg

This topic has been closed for replies.

1 reply

ST Technical Moderator
November 26, 2020

Hello @spark​ ,

Configure the LCD back-light control (LCD_BL_CTRL) via PK3 pin. (You can check the STM32F746 schematic). 0693W000005CpP7QAK.jpgEnable the LCD display using the BSP_LCD_DisplayOn() function:

STM32Cube_FW_F7_V1.16.0\Drivers\BSP\STM32746G-Discovery\stm32746g_discovery_lcd.c

Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks