4 full bridges in parallel using 2 L6206 devices.
Hello
I need to put 4 full bridges in parallel to avoid excessive heat of the L6206
My design is based on figure 15 of the datasheet :
- half bridge 1A connected with half bridge 1B ( pin OUT and pin IN)
- half bridge 2A connected with half bridge 2B ( pin OUT and pin IN)
The same is done with the second device, half bridge 1A-1B of both devices are connected together. Half bridge 2A-2B of both devices are connected together.
The 4RCL resistor are 15k resistor. ( 1.5A for each bridge)
Each OCD pin are connected together
The result should be one full bridge which should allow a current of 6A.
But the current limiting seems not to work correctly. The current is limited to 4.2A in PWM:
IN1A is connected to 5V and a PWM is applied to IN2A. On each rising edge of the PWM ( end of the active phase of the PWM), the OCD make the signal on the Enable pins go down during 300ns. Then the voltage on the Enable pin rises slowly until the next rising edge of the PWM
If I connect IN2A to gnd instead of using a PWM, the current limiting works fine, with a current limited to 5.8A
Has anyone tried to put bridges from different devices in parallel, like I did?