Skip to main content
DWind.1
Associate II
November 23, 2020
Solved

Algobuilder flexible number of properties

  • November 23, 2020
  • 1 reply
  • 888 views

Hi!

I am using Algobuilder and I tried to use a flexible number of properties (like for example in the "Graph"). Although undocumented, I saw in the library for the display that there are <DisplayDependency> and <DisplayCondition> tags. I tried to use them in a custom block, but unfortunately the user interface is not automatically updated when changing the number and the input fields for the properties do not appear.

It is working if I set a value and reload the entire functin block design or the library in algobuilder.

Is this a bug or is this feature simply not supported by custom made blocks?

Best wishes,

Dominik

    This topic has been closed for replies.
    Best answer by Miroslav BATEK

    Hello Dominik,

    we din't expect this will be used by users custom made blocks.

    But it should work except the properties are not automatically updated. You need to deselect the function block and select it again to refresh the properties table.

    We will try fix it in the next version of AlgoBuilder.

    1 reply

    Miroslav BATEKBest answer
    ST Employee
    November 23, 2020

    Hello Dominik,

    we din't expect this will be used by users custom made blocks.

    But it should work except the properties are not automatically updated. You need to deselect the function block and select it again to refresh the properties table.

    We will try fix it in the next version of AlgoBuilder.