Question
RTC and battery
Hey,
If a power off occurs, I would like that the RTC function will keep alive, until Power on.
As I understand, i should connect a coin battery 3.0 to VBAT pin.
My questions are:
- when power is on, does the VBAT PIN supplies from VDD (P3V3) or from the VBAT connected? Or should I connect both on the same line with diodes
- when power goes low, the switch is automatically?
- in case I want only the RTC function when power off, what is the current consumption? Is the 32khz oscillator is used? So the 32khz oscillator should be supplied from vbat too?