How to set up torque control to keep the constant torque regaldress of motor load
Hi,
I have a problem with STM Motor Control,
I got Nucleo F446 and G431 and IHM08M1 motor driver with Maxon EC90 and T-Motor, with Hall sensor encoder.
The problem is, when I set the torque it is hold to certain load. If motor load is greather than motor can carry, the controller reduces PWM duty, and the current and torque drops to almost zero. Is this normal behavior?
Another problem is holding motor in torque control loop. I need to set a torque not only to move a motor, but to hold it in place (aka stationary joint), but when torque is set to only match load, motor instead of holding in place, with constant force it jumps back and forward. Switchig beetwenn phases.
I managed to design a fix to the first issue inside the PWM_Curr_Feedback, but it is not the solution i want. I still did not solved second problem.
Is this designed behavior of Motor Control?