Skip to main content
TSidd.3
Associate
November 21, 2020
Question

Is there an example of reading and using audio from the on-board microphone of the STM32F469I Discovery kit? Details below

  • November 21, 2020
  • 5 replies
  • 2027 views

I am trying to access and read audio from the on-board microphone of my board and run it through a speech recognition model (Tensorflow lite speech commands). I am unable to find the audio library for my board or an example of accessing and using audio from the board. I was wondering if the STM32CubeIDE environment has such an example for this board? Please let me know and your help would be highly appreciated.

This topic has been closed for replies.

5 replies

Dmato.11
Associate
November 21, 2020

I'm looking for also.

KObir.1
Associate II
November 22, 2020

Further to @Community member​ 's tip, to get access to sample written and running example applications - including audio etc - for any of the discovery boards - please download and review the contents of the relevant STM32Cube[F, H ...] firmware file for that board, here the F4 -> STM32CubeF4 - in this case since the STM32F469.... board is an F4 based board. The file will look something like this en.STM32Cube_FW_F4.... for English. Please note that the examples may not necessarily be a full implementation of what you could be looking for

HTH

Gipsyblues

TSidd.3
TSidd.3Author
Associate
November 23, 2020

Thank you for the suggestion. I will see if I can find an example application that can be adopted for my purposes. I would like to ask one more question. Is there an existing audio library for my board? For example the STM32F746 board has the following audio library files 'AUDIO_DISCO_F746NG.h' and 'AUDIO_DISCO_F746NG.cpp' at the following link: https://os.mbed.com/teams/ST/code/AUDIO_DISCO_F746NG/

These files can be used to access and read audio from the F7 board's microphone. If there is are similar files for my board (disco_F469ni), I should be able to use it similarly. Please let me know.