Skip to main content
MatteoFeatureJam
Associate II
November 20, 2020
Question

Which firmware should I use for a SPBTLE-1S?

  • November 20, 2020
  • 0 replies
  • 551 views

I'm using the SPBTLE-1S BlueNRG-1 module on a custom PCB with a STM32L4R9ZI MCU. The SPBTLE-1S module and the main MCU are connected trough SPI. The SPBTLE-1S module can be flashed with various firmwares provided by ST. Which one should i choose? I would like to have it compatible with the code generated by the X-CUBE-BLE1 pack on CubeMX.

    This topic has been closed for replies.