Skip to main content
victagayun
Senior III
November 20, 2020
Solved

Demos not running on STM32F769i-DISCO on Cubeprogrammer 2.6.0

  • November 20, 2020
  • 4 replies
  • 1357 views

Hi,

Almost all demos are not able to run and display on STM32F769i-DISCO using v2.6.0.

Below is the terminal log

You may also refer to https://community.st.com/s/question/0D53W00000O1KHJSA3/run-target-on-stm32h747idisco-failed

Run Target
 Generate
 Done
 Generate Assets
 make -f simulator/gcc/Makefile assets -j8
 Reading ./application.config
 Done
 Post Generate
 touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
 Done
 Post Generate Target
 touchgfx update_project --project-file=../STM32F769I_DISCO.ioc --platform=m7
 Done
 Compile
 make -f ../gcc/Makefile -j8
 Reading TouchGFX/application.config
 Linking TouchGFX/build/bin/target.elf
 Producing additional output formats...
 target.hex - Combined internal+external hex
 intflash.elf - Internal flash, elf debug
 intflash.hex - Internal flash, hex
 extflash.bin - External flash, binary
 Done
 Flash
 make -f ../gcc/Makefile flash
 Reading TouchGFX/application.config
 Linking TouchGFX/build/bin/target.elf
 Producing additional output formats...
 target.hex - Combined internal+external hex
 intflash.elf - Internal flash, elf debug
 intflash.hex - Internal flash, hex
 extflash.bin - External flash, binary
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.6.0 
 -------------------------------------------------------------------
 
 Error: External loader C:\Program cannot be loaded.
 Error: External loader Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader\MX25L512G_STM32F769I-DISCO.stldr cannot be loaded.
 Error: No debug probe detected.
 make[1]: *** [_extflash_] Error 1
 gcc/Makefile:295: recipe for target '_extflash_' failed
 ../gcc/Makefile:53: recipe for target 'flash' failed
 make: *** [flash] Error 2
 Failed
 Failed

This topic has been closed for replies.
Best answer by victagayun

I used cubeprogrammer 2.5 instead, as per

https://community.st.com/s/feed/0D53W00000O1KHJSA3

4 replies

Houda GHABRI
ST Employee
December 10, 2020

Hi @victagayun​ ,

There is a known issue in STM32CubeProgrammer v2.6.0 with paths containing spaces.

what's working with v2.6 :

1- open a CMD (windows command line) in STM32CubeProgrammer bin folder.

2- copy your hex in bin folder.

2- Call CLI in this way : STM32_Programmer_CLI.exe -c port=swd -d Firmware.hex -el ExternalLoader/ExternalLoader.stldr (replace ExternalLoader.stldr with the desired external loader);

You can also use the GUI for downloading your hex.

Hope it helps you.

Houda

Houda GHABRI
ST Employee
December 15, 2020

Hi @victagayun​ ,

I hope my suggestion helps you to run your Demo.

If your question is answered, please close this topic by choosing Select as Best to. This will help other users find that answer faster.

Houda

Tesla DeLorean
Guru
December 15, 2020

Not being able to run out of their default installation directory doesn't seem like a satisfactory solution.

Surely the calling app should be quoting the passed path?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..