Skip to main content
Nikita91
Lead II
November 17, 2020
Solved

How to change STM32CubeMX Firmware repositort folder ?

  • November 17, 2020
  • 2 replies
  • 2412 views

I have STM32CubeMX and STM32CubeIDE installed, but each use a different Firmware repositort folder.

So I have to download (with a slow ADSL line) and install twice every firmware package.

I want to install the package in a directory out of C:/users/Admin because I doesn't have the right to search in these directories.

The repository path and button is grayed in the Updater settings:

0693W000005BfTuQAK.pngWhat can I do ?

Thanks.

This topic has been closed for replies.
Best answer by Khouloud ZEMMELI

Hello @Nikita91​ ,

The Repository Folder could not be changed while a project is open, to change it just after you opened the STM32CubeMX tool (help / updater settings) before creating you project.

Best Regards,

Khouloud

2 replies

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
November 17, 2020

Hello @Nikita91​ ,

The Repository Folder could not be changed while a project is open, to change it just after you opened the STM32CubeMX tool (help / updater settings) before creating you project.

Best Regards,

Khouloud

Cartu38 OpenDev
Graduate II
November 17, 2020

STM32CubeMX is allowing you to update firmware repository thru Help > Updater Settings.

Same is doable if STM32CubeIDE Thanks Windows > Preferences

0693W000005BhhZQAS.jpg 

Obviously you can point to same shared folder. Good pratice would be to avoid any special or blank char within such path.

Thanks to tag answer as best if happy about. It will help community to dig quickly into valuable material.