Skip to main content
turboscrew
Senior III
November 12, 2020
Question

Extra clock pulses with slow SPI master.

  • November 12, 2020
  • 11 replies
  • 2376 views

I wonder if there is some known issue?

With logic analyzer I confirmed that I had extra clock pulses in the SPI after the data was read.

The chip is STM32F427@180MHz.

PCLK2 is 90 MHz

SPI4 (master) is used with 16 bits and with prescaler 64, half duplex, single data line.

I'm reading two 16-bit words with HAL_SPI_Receive(), and after it returns, I turn NSS high.

What I saw with logic analyzer was that after NSS goes high, there were still 16 clock pulses coming out.

When I changed the prescaler even bigger (128), there were no more extra clock pulses.

The chip in the other end has 2 MHz maximum SPI clock.

More accurately:

  • chip select LOW
  • write 16-bit read command with HAL_SPI_Transmit()
  • while receiver is not empty, read DR
  • read two 16-bit values with HAL_SPI_Receive()
  • chip select HIGH
  • 16 extra clock pulses seen

This topic has been closed for replies.

11 replies

TDK
November 12, 2020

Is it a one or two-line master?

> while receiver is not empty, read DR

What is this supposed to do?

"If you feel a post has answered your question, please click ""Accept as Solution""."
turboscrew
Senior III
November 12, 2020

Like I mentioned: half duplex, single data line.

The read just removes old crap that may be left there, before reading the data.

TDK
November 12, 2020

Ahh, I did look but I missed it. Extra clocks in this mode are a recurring issue. The problem is that clocks are sent automatically when RXNE is not asserted, and HAL doesn't stop the transfer until after reading everything, so RXNE is not asserted at the end.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
November 13, 2020

> The problem is that clocks are sent automatically when RXNE is not asserted,

Are you sure it has anything to do with RXNE? IMO it just churns out clocks - multiples of Data Size - as long as SPE is set.

JW

turboscrew
Senior III
November 13, 2020

And why does it happen, if prescaler is 64, but not if prescaler is 128? Also note, that I'm using polling HAL-call for receive.

TDK
November 13, 2020

> Are you sure it has anything to do with RXNE? IMO it just churns out clocks - multiples of Data Size - as long as SPE is set.

You could be right. I'm not very familiar with that mode.

> And why does it happen, if prescaler is 64, but not if prescaler is 128?

It's a race condition in the code. If the rate is slow enough so the CPU finishes first, then you don't get extra clocks.

"If you feel a post has answered your question, please click ""Accept as Solution""."
turboscrew
Senior III
November 13, 2020

So the bug is in HAL, not in HW?

(I still doubt that.)

TDK
November 13, 2020

You can't call it a hardware bug if it's working as described in the RM.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
November 20, 2020

HAL doesn't care. They just enable SPI, wait the specified numbers of frame and disable SPI. As HAL doesn't care to be precise, the disable comes too late, hardware already started to receive the next frame.

JW

turboscrew
Senior III
November 22, 2020

One would think giving the count and using blocking transfer should do...