Skip to main content
DXian
Associate
November 4, 2020
Solved

stm32wrapper4dbg not found when compile TF-A

  • November 4, 2020
  • 2 replies
  • 1793 views

I executed the following command in linux system:

make -f Makefile.sdk all TF_A_CONFIG=trusted FTA_DEVICETREE=stm32mp15c-ev1

but there is the following fault information:

/bin/sh: 22: stm32wrapper4dbg: not found

I have a try to install it, this is not successful. (sudo spt-get install stm32wrapper4dbg)

How to fix this question?

0693W000005AGsJQAW.png

This topic has been closed for replies.
Best answer by OlivierK

Hello DXian (Community Member)

Using the latest available image (openSTLinux 2.0.0), no issues on my side.

Have you correctly installed the SDK and sourced the SDK env?

stm32wrapper4dbg is found here <STM32MPU-Release-20-06-24>/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/stm32wrapper4dbg

Generate /home/osboxes/Desktop/working/STM32MPU-Release-20-06-24/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.2.r1-r0/tf-a-stm32mp-2.2.r1/../build/trusted/tf-a-stm32mp157c-ev1.stm32

Image Type  : ST Microelectronics STM32 V1.0

Image Size  : 241728 bytes

Image Load  : 0x2ffc2500

Entry Point : 0x2ffd6000

Checksum    : 0x00e4ce4c

Option    : 0x00000001

Version   : 0x00000000

Building stm32mp1

make[1]: Leaving directory '/home/osboxes/Desktop/working/STM32MPU-Release-20-06-24/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.2.r1-r0/tf-a-stm32mp-2.2.r1'

Image Type  : ST Microelectronics STM32 V1.0

Image Size  : 241784 bytes

Image Load  : 0x2ffc2500

Entry Point : 0x2fffd541

Checksum    : 0x00e4e4e7

Option      : 0x00000001

Version     : 0x00000000

Halt Address : 0x2ffd6000

2 replies

OlivierK
OlivierKBest answer
ST Technical Moderator
November 17, 2020

Hello DXian (Community Member)

Using the latest available image (openSTLinux 2.0.0), no issues on my side.

Have you correctly installed the SDK and sourced the SDK env?

stm32wrapper4dbg is found here <STM32MPU-Release-20-06-24>/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/stm32wrapper4dbg

Generate /home/osboxes/Desktop/working/STM32MPU-Release-20-06-24/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.2.r1-r0/tf-a-stm32mp-2.2.r1/../build/trusted/tf-a-stm32mp157c-ev1.stm32

Image Type  : ST Microelectronics STM32 V1.0

Image Size  : 241728 bytes

Image Load  : 0x2ffc2500

Entry Point : 0x2ffd6000

Checksum    : 0x00e4ce4c

Option    : 0x00000001

Version   : 0x00000000

Building stm32mp1

make[1]: Leaving directory '/home/osboxes/Desktop/working/STM32MPU-Release-20-06-24/Developer-Package/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.2.r1-r0/tf-a-stm32mp-2.2.r1'

Image Type  : ST Microelectronics STM32 V1.0

Image Size  : 241784 bytes

Image Load  : 0x2ffc2500

Entry Point : 0x2fffd541

Checksum    : 0x00e4e4e7

Option      : 0x00000001

Version     : 0x00000000

Halt Address : 0x2ffd6000

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
DXian
DXianAuthor
Associate
November 18, 2020

Thanks for your reply. I will re-install all software.