Skip to main content
SPark.15
Associate III
November 4, 2020
Question

Hotspot mode problem using hostapd in STM32MP157C-DK2.

  • November 4, 2020
  • 2 replies
  • 1283 views

Hello Guys.

I am using STM32MP157C-DK2 and st-image-core.

Looking at the st-image-weston and wiki Page, I am configuring the hotspot mode to be available in my image.

First, while looking at the wiki page and st-image-weston, I composed a script that uses the following command.

(/usr/sbin/hostapd /etc/hostapd.conf -P /run/hostapd.pid -B)

I created systemd because there is no response from the installed hostapd systemd.

Next, I made systemd execute my script.

However, the hotspot mode did not work.

If I run the script directly from the terminal or crontab, hotspot mode operates normally as shown below.

---------------------------------------------------------------

Configuration file: /etc/hostapd.conf

wlan0: Could not connect to kernel driver

Using interface wlan0 with hwaddr 10:98:c3:63:a7:e3 and ssid "HSGT_SsgRk4hU"

random: Only 19/20 bytes of strong random data available

random: Not enough entropy pool available for secure operations

WPA: Not enough entropy in random pool for secure operations - update keys later when the first station connects

wlan0: interface state UNINITIALIZED->ENABLED

wlan0: AP-ENABLED

wlan0   Link encap:Ethernet HWaddr 10:98:C3:63:A7:E3

     inet addr:192.168.72.1 Bcast:192.168.72.255 Mask:255.255.255.0

     inet6 addr: fe80::1298:c3ff:fe63:a7e3/64 Scope:Link

     UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1

     RX packets:0 errors:0 dropped:0 overruns:0 frame:0

     TX packets:1142 errors:0 dropped:0 overruns:0 carrier:0

     collisions:0 txqueuelen:1000

     RX bytes:0 (0.0 B) TX bytes:197392 (192.7 KiB)

---------------------------------------------------------------

However, if I run it from systemd, it will not run with the following message.

----------------------------------------------------------------

Could not set channel for kernel driver

Interface initialization failed

wlan0: interface state UNINITIALIZED->DISABLED

wlan0: AP-DISABLED

wlan0: Unable to setup interface.

wlan0: interface state DISABLED->DISABLED

wlan0: AP-DISABLED

wlan0: CTRL-EVENT-TERMINATING

hostapd_free_hapd_data: Interface wlan0 wasn't started

nl80211: deinit ifname=wlan0 disabled_11b_rates=0

----------------------------------------------------------------

Or, it appears as if it succeeded as below, but it is not actually applied in ifconfig.

----------------------------------------------------------------

current no hotspot mode -> hotspot start

Configuration file: /etc/hostapd.conf

wlan0: Could not connect to kernel driver

Using interface wlan0 with hwaddr 10:98:c3:63:a7:e3 and ssid "HSGT_SsgRk4hU"

wlan0: interface state UNINITIALIZED->ENABLED

wlan0: AP-ENABLED

Hotspot mode start success

wlan0   Link encap:Ethernet HWaddr 10:98:C3:63:A7:E3

     inet6 addr: fe80::1298:c3ff:fe63:a7e3/64 Scope:Link

     UP BROADCAST MULTICAST MTU:1500 Metric:1

     RX packets:0 errors:0 dropped:0 overruns:0 frame:0

     TX packets:8 errors:0 dropped:0 overruns:0 carrier:0

     collisions:0 txqueuelen:1000

     RX bytes:0 (0.0 B) TX bytes:1289 (1.2 KiB)

----------------------------------------------------------------

How can I solve this problem? Can't I run it with the commands listed above?

If there is any other way, please let me know.

In addition, the script I configured is composed as follows.

It is designed to simply search for IP and execute the command if it does not exist.

-----------------------------------------------------------------

#!/bin/sh

status=`/sbin/ifconfig | grep 192.168.72.1 | wc -l`

if [ $status -gt 0 ]

then

    echo "current hotspot mode -> skip"

else

    echo "no hotspot mode -> hotspot start"

    /usr/sbin/hostapd /etc/hostapd.conf -P /run/hostapd.pid -B > /home/root/result.txt

    status_again=`/sbin/ifconfig | grep 192.168.72.1 | wc -l`

    if [ $status_again -gt 0 ]

    then

        echo "Hotspot mode start success"

    else

        echo "Hotspot mode start fail"

    fi

fi

-----------------------------------------------------------------

thanks

This topic has been closed for replies.

2 replies

Christophe Guibout
ST Technical Moderator
November 25, 2020

Hi @SPark.15​ ,

I think you don't need to create a new service that manages hostapd, as hostapd service already does the job. You only need to update /etc/default/hostapd according with your needs, and restart the related services.

I would recommand to have a look into st-hotspot-wifi-service.sh script which already manage this (on target : /usr/local/demo/bin)

Please also cross-check that the network file is correct :

root@stm32mp1:~# networkctl status wlan0
 Link File: /lib/systemd/network/99-default.link 
Network File: /lib/systemd/network/hostapd.network 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SPark.15
SPark.15Author
Associate III
December 18, 2020

I understood what you say. I check that script you said(st-hotspot-wifi-service.sh).

​I understood that after updating hostapd.network as I want, And restart the hostapd service.

I try that you recommend.

Thank you for your help