Skip to main content
Darshan Patel
Associate II
November 3, 2020
Question

Motor Profiler failure with IMP20B and Nucleo Board F302R8

  • November 3, 2020
  • 9 replies
  • 3552 views

I have IMP20B with Nucleo Board F302R8.

I tried with Motor Profiler. In over current small dot shows red and profile failed.

With same configurations i tried once & motor runs a bit.

0693W000005A8KnQAK.png

This topic has been closed for replies.

9 replies

Laurent Ca...
Senior III
November 3, 2020

Dear @Community member​ 

To respect the forum rules for the "STM32 Motor Control" tag, I moved your entire title to the description part of the text, and shortened your title.

Best regards

Laurent Ca...

Darshan Patel
Associate II
November 3, 2020

Sorry will take care of that from now onwards

Laurent Ca...
Senior III
November 3, 2020

Dear @Community member​ 

Sorry but I do not understand very well your sentence "In over current small dot shows red and profile failed."

Best regards

Laurent Ca...

Darshan Patel
Associate II
November 3, 2020

0693W000005A8mIQAS.png

Darshan Patel
Associate II
November 3, 2020

Hello Just Zoom the corner Faults Section, Its due to External SMPS???

Dario CUCCHI
ST Employee
November 30, 2020

Hi Darshan,

I'm here following the link in this previous post.

I see from the screenshot the board selected in the profiler is IPM15B.

However you mentioned that you have a IPM20B. Do you confirm ?

If so, consider that the two boards are different, so maybe it could be the cause of this issue.

Moreover, even without any error, using a different board bring to an incorrect profiling of the motor values.

Darshan Patel
Associate II
December 1, 2020

Yes you are right i used IPM20B instead of IPM15B.

I agree with your feedback with using IPM15B. but motor once runs for few seconds.

I ordered IPM15 already.

Laurent Ca...
Senior III
June 28, 2021

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards