Skip to main content
GErma.1
Associate III
November 2, 2020
Solved

ST25DV64K-IER6S3 - GPO Operation (open drain)

  • November 2, 2020
  • 2 replies
  • 687 views

Hi

I am trying to obtain the smallest possible power consumption with an ST25DV64K-IER6S3 device. I am wondering is the GPO pin is still operational when VCC is removed? Is it the GPO circuit powered by the RF interface?

Best Regards

Gilberto

    This topic has been closed for replies.
    Best answer by JL. Lebon

    ​Hello,

    Yes, GPO is triggered independently from VCC.

    In absence of VCC, the GPO logic is powered by the RF field.

    On the Open drain version of the ST25DV (St25DV64K-IE6S3), the GPO output is open drain, which means it needs to have an external pull-up resistor connected to it in order to work. This pull-up must be powered somehow by an external power source (VCC, or even energy harvesting).

    Best regards.

    2 replies

    GErma.1
    GErma.1Author
    Associate III
    November 2, 2020

    Hi

    I have managed to run some testing with ST25 APP from ST. It seems that GPO is triggered independently of VCC. Just need need to confirm that.

    BR

    Gilberto

    JL. Lebon
    JL. LebonBest answer
    ST Employee
    November 3, 2020

    ​Hello,

    Yes, GPO is triggered independently from VCC.

    In absence of VCC, the GPO logic is powered by the RF field.

    On the Open drain version of the ST25DV (St25DV64K-IE6S3), the GPO output is open drain, which means it needs to have an external pull-up resistor connected to it in order to work. This pull-up must be powered somehow by an external power source (VCC, or even energy harvesting).

    Best regards.