Associate III
Nov 1, 2020 10:16 PM UTC
Question
Why the source file are missing when import an existing projects into workspace?
- 7 replies
- 3386 views
I'm trying to importo into the workspace the GPIO Example for L010RB.
I go on File -> Import ... -> and select "Import existing project into workspace"
In root folder insert:
C:\Users\****\STM32Cube\Repository\STM32Cube_FW_L0_V1.11.3\Projects\NUCLEO-L010RB\Examples\GPIO
And check the single project present into "Project:"
I check "copy projects into workspace" and then "Finish" ( see attached STM_import).
At this point, I see the project into the workspace, but the source file are not present (see attacched STM_Project).
What is the correct way to import an existing project?
Thanks.