Skip to main content
SS_135
Associate
October 20, 2020
Question

Unicleo-GUI -FFT size issue

Hi Team,

Customer is using X-Nucleo-IKS02A1 board to test the vibration sensor using vibration monitoring example code. The FFT data of vibration sensor is observed using Unicleo-GUI.

Vibration Monitoring example code works fine with FFT size of 512. But does not work with FFT size of more than 512.

It is observed that the FFT data is not represented in Unicleo-GUI when FFT size is changed from FFT_SIZE_512 FFT_SIZE_1024 in MotionSP_Config.h file.

Please suggest the configuration settings to increase FFT size.

Regards

    This topic has been closed for replies.

    4 replies

    Ozone
    Principal
    October 20, 2020

    > Vibration Monitoring example code works fine with FFT size of 512. But does not work with FFT size of more than 512.

    So, I suggest to inspect the example code, and adapt it for a different FFT size.

    The free-to-use and free-of-charge examples are usually not tuned to fit every possible customers need.

    I did that for SPL-based FFT example some while ago, and it took me less than one afternoon.

    Rajesh1
    Associate III
    October 26, 2020

    Hi Ozone,

    Can you please share us the SPL-based FFT example which shall be used as reference to us.

    Regards,

    Rajesh K.

    Eleon BORLINI
    ST Employee
    October 26, 2020

    @Rajesh​ , please note in general that the audio FFT is a little different from the motion MEMS FFT (vibration sensors on the X-Nucleo-IKS02A1), since audio PCM is not limited by a FIFO (microphone has no embedded FIFO).

    -Eleon

    Eleon BORLINI
    ST Employee
    October 21, 2020

    Hi,

    you can please refer to this topic for this question.

    -Eleon