Question
Why my convertion time is not correct when the sampling time is less than 84 Sampling time ?
Hello,
I'm using STM32f411RE with ADC and I would like to know why when the sampling time is less than 84, I don't find by calculation the same expected conversion frequency/time?
My calculation is Tconv = (3+12)/210000Hz = 714 ns so a frequency of 1.4 MHz. But in the measurement, I find a frequency of 260 kHz:
Here is my program:
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 1);
HAL_GPIO_TogglePin(GPIOA, LD2_Pin);
res = HAL_ADC_GetValue(&hadc1);
res = res * 3.3/4095;
}
/* USER CODE END 3 */I use a led with the toggle function after each conversion.
Thank you in advance for your help.