Skip to main content
CSern.1
Associate
October 16, 2020
Question

STMCubeMX - "Pin compatible feature" bug reporting.

  • October 16, 2020
  • 6 replies
  • 2211 views

Hi everyone,

We have discovered a bug with the STMCubeMX'S Pinout compatible feature between STM32F030C8 and STM32F030CC.

  • Based on the STMCubeMX both MCUs (STM32F030C8 and STM32F030CC) are Full Pinout Compatible.
  • Based on the STM32F030 datasheet, there are differences on pins #35 and #36 (LQFP48 package).

Attaching images for your reference.

Thank you,

PS. We have create some prototypes assuming both MCU are fully pinout compatible but, after HW troubleshooting, we had to use some jumpers/wires to solve this pinout incompatibility issue.

This topic has been closed for replies.

6 replies

Nesrine.JLASSI
Visitor II
October 19, 2020

Hi @Carlos Andrés Serna Anduquia​ 

Could you please specify the datasheet version you are using.

I checked in the datasheet DS9773 Rev 4, Figure 5 shows LQFP64 64-pin package pinout (top view), for STM32F030RC devices not STM32F030CC. So, i think that the issue (solved) occurs at the datasheet not STM32CubeMX.

0693W000004KHt9QAG.pngBest regards,

Nesrine

ST Technical Moderator
October 21, 2020

Hi @Carlos Andrés Serna Anduquia​ ,

If the answer of Nesrine answered your question, please mark it as "best answer".

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
CSern.1
CSern.1Author
Associate
October 21, 2020

Hi @Nesrine.JLASSI​,

We are using the same datasheet you have checked (DS9773 Rev 4).

As you can see, figures #6 and #7 show a pinout difference between STM32F030C8 and STM32F030CC.

The confusion/issue is on STMCubeMX, If you compare both MCUs (STM32F030C8 and STM32F030CC) using the STMCubeMX, both are classified as "full pinout compatible", as shown in the image right below:

Issue: There is an incongruence on STMCubeMX, these MCUs (STM32F030C8 and STM32F030CC) should not be classified as "full pinout compatible" based on datasheet (DS9773 Rev 4).

Q. Are we using the STMCubeMX wrong? or Is the issue located on the SMTCubeMX ?

@Imen DAHMEN​ , the question has not been answered yet :grinning_face_with_sweat: .

CSern.1
CSern.1Author
Associate
October 21, 2020

PS. The system did not allow me to add the images on my last comment, please find attached them in the following link:

https://photos.app.goo.gl/CFDDya5fw6J4G7yJ8

Nesrine.JLASSI
Visitor II
October 22, 2020

Hi @Carlos Andrés Serna Anduquia​ 

Thanks for your post. I have raised your feedback internally to be reviewed and treated accordingly to the priority. We will give you an update as soon as possible.

Thanks for your contribution

Best regards,

Nesrine

CSern.1
CSern.1Author
Associate
October 22, 2020

Noted @Nesrine.JLASSI​ , Thanks for your attention.

Best regards.