Skip to main content
M4R10
Associate III
October 15, 2020
Question

STM32L496: Unable to go in DFU when use HAL_SPI_Transmit_DMA

  • October 15, 2020
  • 2 replies
  • 704 views

Hello guys,

I'm not new using DFU but I have this strange problem.

When I try to jump in DFU from my code, I get an "Unknown usb device" from my PC.

I have also 2 push button in my board. Reset and DFU pin (keep PH3 high ).

If I keep pressed DFU button and then pressing Reset it fall in the same state (Unknown device).

If I keep pressed DFU button and plug the usb (I get the power from usb) it works.

Investigating I discovered that commenting this line

HAL_SPI_Transmit_DMA(&hspi1,(uint8_t *)bProgADC,sizeof(bProgADC));

DFU works in every case.

What is very strange is that resetting MCU while keep pressed DFU button is not enough, I must cut the power and plug the usb cable while pressing DFU button to go in DFU.

While commenting that SPI line everything is fine

How HAL_SPI_Transmit_DMA can cause this?

How can I fix it?

Thanks in advance

--

Mario

This topic has been closed for replies.

2 replies

TDK
October 16, 2020

Does your program use the USB at all? Are any other bootloader peripherals active during reset, possibly the SPI? What exactly does the DFU button do?

"If you feel a post has answered your question, please click ""Accept as Solution""."
M4R10
M4R10Author
Associate III
October 16, 2020

My program use USB. It is configured as VCP

Bootloader peripheral are USB, USART1 and SPI1. When I jump to DFU from code I tried to stop/disable everything but still the same issue.

DFU button link PH3 to VCC. Pushbuttons are working, I checked with oscilloscope.