Skip to main content
S_L
Visitor II
October 15, 2020
Question

headless-build JVM terminated

First of all, I want to ask whether my use case is achievable with headless-build:

I want to build my project (with frequently changing files and directories) from terminal

[In Terminal]: [Project]/Release: make -j12 all

When I change some source files including folders inside src, this command is not working anymore (sources.mk and so on are outdated). That's why I think I have to call headless build to update makefile, sources.mk etc.

Here's my problem when I call headless-build. I had a look on all threads with search hit on headless, but non helped me (if I understood them correctly).

/opt/st/stm32cubeide_1.4.0$ ./headless-build.sh -build LWC_STM -data /home/sl/Programming/STM14/

[-Dosgi.requiredJavaVersion=1.8, -Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.4.0, -Declipse.buildId=Version 1.4.0, -XX:+UseG1GC, -XX:+UseStringDeduplication, -Xms256m, -Xmx1024m, -build, LWC_STM]

Error: Unknown argument: -Dosgi.requiredJavaVersion=1.8

Usage: 

  -import   {[uri:/]/path/to/project}

  -importAll {[uri:/]/path/to/projectTreeURI} Import all projects under URI

  -build   {project_name_reg_ex{/config_reg_ex} | all}

  -cleanBuild {project_name_reg_ex{/config_reg_ex} | all}

  -no-indexer Disable indexer

  -markerType Marker types to fail build on {all | cdt | marker_id}

  -printErrorMarkers Print all error markers

  -I     {include_path} additional include_path to add to tools

  -include  {include_file} additional include_file to pass to tools

  -D     {prepoc_define} addition preprocessor defines to pass to the tools

  -E     {var=value} replace/add value to environment variable when running all tools

  -Ea     {var=value} append value to environment variable when running all tools

  -Ep     {var=value} prepend value to environment variable when running all tools

  -Er     {var} remove/unset the given environment variable

  -T     {toolid} {optionid=value} replace a tool option value in each configuration built

  -Ta     {toolid} {optionid=value} append to a tool option value in each configuration built

  -Tp     {toolid} {optionid=value} prepend to a tool option value in each configuration built

  -Tr     {toolid} {optionid=value} remove a tool option value in each configuration built

        Tool option values are parsed as a string, comma separated list of strings or a boolean based on the option's type 

Saving workspace.

Stm32cubeide:

JVM terminated. Exit code=1

/opt/st/stm32cubeide_1.4.0/jre/bin/java

-jar /opt/st/stm32cubeide_1.4.0//plugins/org.eclipse.equinox.launcher_1.5.500.v20190715-1310.jar

-os linux

-ws gtk

-arch x86_64

-launcher /opt/st/stm32cubeide_1.4.0/stm32cubeide

-name Stm32cubeide

--launcher.library /opt/st/stm32cubeide_1.4.0//plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.1100.v20190907-0426/eclipse_1801.so

-startup /opt/st/stm32cubeide_1.4.0//plugins/org.eclipse.equinox.launcher_1.5.500.v20190715-1310.jar

--launcher.overrideVmargs

-exitdata 28044

-Dosgi.requiredJavaVersion=1.8

-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.4.0

-Declipse.buildId=Version 1.4.0

-XX:+UseG1GC

-XX:+UseStringDeduplication

-Xms256m

-Xmx1024m

-application org.eclipse.cdt.managedbuilder.core.headlessbuild

-build LWC_STM

-data /home/sl/Programming/STM14/

-vm /opt/st/stm32cubeide_1.4.0/jre/bin/java

-vmargs

-jar /opt/st/stm32cubeide_1.4.0//plugins/org.eclipse.equinox.launcher_1.5.500.v20190715-1310.jar

My system: Linux Mint 19.3 Tricia

java --version

openjdk 11.0.8 2020-07-14

OpenJDK Runtime Environment (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1)

OpenJDK 64-Bit Server VM (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1, mixed mode, sharing)

which java

/usr/bin/java

This topic has been closed for replies.