Skip to main content
kalvacherla.chandrashekhar
Associate III
October 15, 2020
Solved

For STM32H745XI-Disco board are there example source code for initializing and using CRC , SDRAM and also using the EMMC 4GB flash .

  • October 15, 2020
  • 2 replies
  • 1055 views

Hi ,

We need to develop driver for 4GB EMMC flash and SDRAM .

For STM32H745XI-Disco board is there example source code for initializing and using CRC , SDRAM and also using the EMMC 4GB flash .

Thanks In Advance

This topic has been closed for replies.

2 replies

waclawek.jan
waclawek.janBest answer
Super User
October 15, 2020
Tesla DeLorean
Guru
October 15, 2020

I suspect there is, but mashing them together will require some attention to detail, usually the clocking choices/combinations ST chose for any of the specific examples. The BSP code packages should be able to be pulled together.

Couple of hours effort, commercial stuff, hire someone

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..