F4 and F7 SPI CLK waveform
During testing an SPI DAC (TI DAC8563) on an STM32F446RE (where it works) and on an STM32F767ZI (where output is always 0V), I noticed a different SPI clock waveform.
In F4 you have three "8 pulses" signals from CLK (the message from MOSI is 24 bit), while in F7 you can read a single 24-pulse signal on CLK. The two programs are quite the same (generated by CubeIDE), so I suspect that the DAC8533 doesn't recognize the different words. The duration of signals are quite the same for the two MCU (10-15us)
This is the F4:

This is the F7:

Then I modified the F7 config to have the same SYNC Low timing (40us) but nothing changed.
Any idea?
Thanks very much,
Mario