Skip to main content
SBS.1
Visitor II
October 7, 2020
Question

On the fly OTA example

  • October 7, 2020
  • 1 reply
  • 790 views

Hi,

I am working on STM32 with Quectel GPRS module.

Now I have to implement OTA without using any external flash or SD card.

Is there any example for GPRS based OTA without using any external memory to park the bin/hex file and program the MCU flash on the fly.

Regards,

Shri

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    October 7, 2020

    Does the modem have it's own mass-storage memory into which it can FTP download the firmware or deltas, and then apply them from there?

    Going to be a tad challenging it you have now way to stage it, and the modem doesn't participate.

    Pretty much you're going to have to read the instructions, and implement the code to perform them.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..