Question
unwind the stack in non-exception
Hello
I have STM32F407VG MCU with STM32CubeIDE
I want to unwind the stack
I've found answers online and I've tried that code
The code works fine after a hardfault happens
I tried to use the same code within running (no fault happens) but couldn't do that
The stack has the exact same value
I unwind the stack inside an IRQ and I want to know where the code was before the IRQ got called
Here's the IRQ code:
void TIM4_IRQHandler(void)
{
/* USER CODE BEGIN TIM4_IRQn 0 */
if(++iwdg_timer >= Get_IWDG_Threshold()){
uint32_t lrStacked[5] = {0};
uint32_t topFp = __get_LR();
uint32_t nextFp = (uint32_t)&topFp;
Stack_Unwind(256, nextFp, lrStacked, 5);
//RTC_Write_LR_Stack(lrStacked);
}
/*
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKUP_WDG_MAX) < iwdg_timer){
HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKUP_WDG_MAX, iwdg_timer);
}
*/
/* USER CODE END TIM4_IRQn 0 */
HAL_TIM_IRQHandler(&htim4);
/* USER CODE BEGIN TIM4_IRQn 1 */
/* USER CODE END TIM4_IRQn 1 */
}
static void Stack_Unwind(uint32_t iteration, uint32_t nextFp, uint32_t *lrStacked, uint32_t size){
/* loop backtrace using lr to unwind the call stack */
for(uint32_t i=0, j=0; i<iteration; i++){
uint32_t lr = *((uint32_t*)nextFp);
if((lr >= 0x08000000) && (lr <= 0x080FFFFF)){
lrStacked[j] = lr;
j++;
}
nextFp = nextFp + 4;
if (nextFp == 0x20020000 || j == size){
break;
}
}
}
__STATIC_FORCEINLINE uint32_t __get_LR(void)
{
uint32_t result;
__ASM volatile ("MOV %0, lr\n" : "=r" (result) );
return(result);
}