Skip to main content
MMoba.1
Visitor II
October 5, 2020
Question

BAUD RATE CALCULATION FOR USART IN STM32

  • October 5, 2020
  • 12 replies
  • 22577 views

PLEASE EXPLAIN WHY 104.167 IS CONVERTED TO 104.1875 AND HOW ITS ENCODED AS 0X683

MY UNDERSTANDING FOR ENCODING IS 104 IS CONVERTED TO HEX AS MANTISSA PART AS DECIMAL TO HEX AND O.1875 IS CONVERTED SEPARATELY FOR FRACTION PART.

IF I USE FCLK/BAUDRATE I.E 16MHZ/9600= 1666.666d =1667d=0x683h

why use above formula i don't understand.

0693W000004IhA6QAK.jpg

This topic has been closed for replies.

12 replies

TDK
October 5, 2020

Because some amount of error is allowed in the USART clock rate, and it's the closest achievable value. Typically under 1% is fine. No clock has perfect accuracy.

104.1875 = 0x683 / 16

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
October 5, 2020

The BRR uses a fixed-point representation, ie Q12.4

int((104.1875 * 16) + 0.5) = 1667 = 0x683

Personally I've been using BRR = APBCLK / BAUD for 13+ years, it is simpler to explain/compute.

You are basically computing the 16x rate, the USART divides the window into 16 pieces, and can realign the input based on the center time of the bit, basically they have a 16-bit shift register on the input, and they use that to recognize the input/edges.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
m-electronics
Graduate
July 7, 2024

Hello, I must write here in 2024 also because I´m want to go sure that I understand your calculating right.
You only divide the APBCLK / BAUD_RATE and write this value into the BRR register? Am I right with this?

waclawek.jan
Super User
July 7, 2024

Which STM32?

As I've said above, with the default 16-times oversampling, yes.

JW

 

waclawek.jan
Super User
October 5, 2020

> Personally I've been using BRR = APBCLK / BAUD for 13+ years, it is simpler to explain/compute.

+1, but the calculation gets more tricky if you want to use the 8x oversampling. OTOH, I'm yet to find a reason for that (except extreme baudrates, which are not a good idea anyway).

JW

waclawek.jan
Super User
July 7, 2024

No.

Oversampling in context of UART means, how many times one bit is sampled. Normally, it's 16x, so the UART's machine has to be clocked at a frequency which is 16x the UART baudrate.

That's what the integer part of the divider ensures; however, the UART clock generator is not integer-divider but fractional-divider (look up either this or "fractional-N divider"). The resulting clock is not entirely regular, but in average it performs quite well even if the APB clock is not integer-divisible by baudrate*16.

The STM32 UART has an optional mode where oversampling is not 16x but 8x, see OVER8 bit.

Read the UART chapter in RM, this is described there.

JW

m-electronics
Graduate
July 8, 2024

I'm understanding now the calculation of the mantissa and fraction and with that the baudrate when it's 16x oversampling.

I guess now that the calculation formula for 8x oversampling is the following:

 

BAUD = fCK / (8 * USARTDIV) ? (And not (16 * USARTDIV))

Am I right with this

And is there any reason for change the oversampling rate?

waclawek.jan
Super User
July 8, 2024

Yes.

> And is there any reason for change the oversampling rate?

In the extreme case of very low AHB/APB clock, you can achieve higher baudrates, at the cost of somewhat lower baud mismatch immunity.

JW

m-electronics
Graduate
July 10, 2024

In the documentation stands something about, if the fraction is too big for the 4 bits then the "carry" must be added to the mantissa.

Screenshot 2024-07-10 at 08.24.17.png

But I don´t understand what the "carry" of 0d0.99 is? Because they simply round up the 0d50.990 to 0d51. :thinking_face: