Skip to main content
Ara.1
Associate III
October 2, 2020
Solved

stm32mp157caa3 galcore.ko

  • October 2, 2020
  • 7 replies
  • 2795 views

Time out check load galcore module expired

whay are we getting this, how to fix this, ?

This topic has been closed for replies.
Best answer by mteaching

I make a try just now, and now it works.

It's not enough to compile the kernel, you also need to compile the module. And you must follow the steps on the wiki.

But "Time out check load galcore module expired" still exits, which results in the USB network card and screen restart. This is too bad.

0693W00000GZ9DXQA1.pnglog

[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Daily apt download activities.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ 11.595874] stm32-crc32 58009000.crc: Initialized
[ 11.647514] galcore: disagrees about version of symbol module_layout
[ 11.759060] Bluetooth: HCI UART driver ver 2.3
[ 11.762136] Bluetooth: HCI UART protocol H4 registered
[ OK ] Listening on dropbear.socket.
[ 11.805211] Bluetooth: HCI UART protocol Broadcom registered
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Kernel Logging Service.
[ OK ] Started System Logging Service.
[ OK ] Started D-Bus System Message Bus.

7 replies

Olivier GALLIEN
ST Technical Moderator
October 5, 2020

Hi @Ara.1​ 

You are giving too few informations about your setup and application to provide pertinent answer.

Please add further detail about what you are doing.

which board ? Custom build ? from Distri, Developper pack etc...

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
ST Technical Moderator
October 5, 2020

Complete boot log and traces around galcore failure is also a must

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ara.1
Ara.1Author
Associate III
October 6, 2020

Hi Olivier,

attached is the current log,

I did rebuild all my custom image once again from wiki st link steps followed, the distro is openst-weston-wayland.

now i can able to see Galcore getting probed.

[  11.165705] galcore: loading out-of-tree module taints kernel.

[  11.235260] Galcore version 6.2.4.190076

how can i test STM32MP1 GPU/galcore.ko functionality ?