Question
Conflicting definition of HAL_DCMI_Init?
I'm experiencing a runtime crash when using DCMI in with `USE_HAL_DCMI_REGISTER_CALLBACKS`.
The crashing lines are
#if (USE_HAL_DCMI_REGISTER_CALLBACKS == 1)
/*Call registered DCMI line event callback*/
hdcmi->LineEventCallback(hdcmi);
#else
HAL_DCMI_LineEventCallback(hdcmi);
#endif /* USE_HAL_DCMI_REGISTER_CALLBACKS */This seems to be caused by by conflicting definitions of `HAL_DCMI_Init`.
One definition is in `stm32f4xx_hal_dcmi.c`:
__weak HAL_StatusTypeDef HAL_DCMI_Init(DCMI_HandleTypeDef *hdcmi)
{
//...
/* Init the DCMI Callback settings */
#if (USE_HAL_DCMI_REGISTER_CALLBACKS == 1)
hdcmi->FrameEventCallback = HAL_DCMI_FrameEventCallback; /* Legacy weak FrameEventCallback */
hdcmi->VsyncEventCallback = HAL_DCMI_VsyncEventCallback; /* Legacy weak VsyncEventCallback */
hdcmi->LineEventCallback = HAL_DCMI_LineEventCallback; /* Legacy weak LineEventCallback */
hdcmi->ErrorCallback = HAL_DCMI_ErrorCallback; /* Legacy weak ErrorCallback */
if(hdcmi->MspInitCallback == NULL)
{
/* Legacy weak MspInit Callback */
hdcmi->MspInitCallback = HAL_DCMI_MspInit;
}
/* Initialize the low level hardware (MSP) */
hdcmi->MspInitCallback(hdcmi);
#else
/* Init the low level hardware : GPIO, CLOCK, NVIC and DMA */
HAL_DCMI_MspInit(hdcmi);
#endif /* (USE_HAL_DCMI_REGISTER_CALLBACKS) */There is a conflicting definition that takes priority in `stm32f4xx_hal_dcmi_ex.c`, since it is not declared `__weak`:
HAL_StatusTypeDef HAL_DCMI_Init(DCMI_HandleTypeDef *hdcmi)This initializer does *not* assign LineEventCallback, and doesn't even mention `USE_HAL_DCMI_REGISTER_CALLBACKS`
What's the deal? Is this user error or a bug in HAL?