What is the L6474 ABS_POS register really reporting?
I am looking at using the L6474 to drive a stepper motor. I have a question about the absolute position register (ABS_POS).
It says it is the current motor absolute position, but I want to clarify that it really is just a counter for the number of steps that have been commanded?
It initializes to 0 at power up, so it has no history, so it is really an incremental counter not an absolute. It also says it is the motor position, but it just keeps track of how many steps have been commanded, correct? There is no feedback from the motor to say if it has really taken the step or not, or if the motor was turned by something other than the motor driver, it wouldn't know, so the "motor absolute position" would be incorrect.
Is that true?