Skip to main content
Sde B.1
Visitor II
September 30, 2020
Question

STM32F722 Bootloader Failure with Low Voltage on VDD pins

  • September 30, 2020
  • 1 reply
  • 902 views

Our team has noticed that with a stock STM32F722RE, and 0.4V applied to the VDD pins (which is occuring in our case due to a 3.3v CAN transceiver), when 3.3V is finally applied to the chip (ie voltage goes from 0.4->3.3V), bootloader entry via USB connection will fail (on ubuntu using the dmesg command we get persistent 'device descriptor read/64, error -32'). This condition persists even if we hardware reset the chip by toggling the reset pin.

If the 0.4V is removed (by disabling the transceiver or momentarily shorting the pins together) and then 3.3V reapplied (0.4->0.0->3.3V) ie a complete power cycle, the stm32 bootloader starts up fine.

Has anyone had a similar problem? On reading the datasheet we cant find any indication that the USB functionality of the chip will fail if VDD is less than the brown-out threshold (~2.5V in our case).

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
September 30, 2020

Where is that 0.4V exactly from? Do you power the mcu parasitically through its IO pins, i.e. is there any significant voltage on any of the pins?

JW