Skip to main content
Hsn
Associate II
September 29, 2020
Question

How to compile the device tree(Cubemx) with the Distribution Package ?

  • September 29, 2020
  • 3 replies
  • 1870 views

I have generated a project with cubemx and tried all the instructions from this article..

https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package

My layer.conf look like this

BBPATH .= ":${LAYERDIR}"
 
 
BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \
 ${LAYERDIR}/recipes-*/*/*.bbappend"
 
BBFILE_COLLECTIONS += "meta-my-demo-layer"
BBFILE_PATTERN_meta-my-demo-layer = "^${LAYERDIR}/"
BBFILE_PRIORITY_meta-my-demo-layer = "6"
EULA_FILE_ST_stm32mpmydemo = "${LAYERDIR}/conf/eula/${MACHINE}"
EULA_FILE_ST_MD5SUM_stm32mpmydemo = "8b505090fb679839cefbcc784afe8ce9"
LICENSE_PATH += "${LAYERDIR}/files/licenses"
STM32MP_MY_DEMO_BASE = "${LAYERDIR}"
 
LAYERVERSION_meta-my-demo-layer = "1"
 
LAYERDEPENDS_meta-my-demo-layer = "stm-st-stm32mp-mx"
 
LAYERVERSION_meta-my-demo-layer = "1"
 
 
LAYERDEPENDS_meta-my-demo-layer = "core"
LAYERSERIES_COMPAT_meta-my-demo-layer = "dunfell"

My machine configurations look like this ...

#@TYPE: Machine
#@NAME: stm32mp1-mx
#@DESCRIPTION: Configuration for STM32CubeMX generated project
#@NEEDED_BSPLAYERS: layers/meta-openembedded/meta-oe layers/meta-openembedded/meta-python layers/meta-st/meta-st-stm32mp-addons
 
include conf/machine/include/st-machine-common-stm32mp.inc
include conf/machine/include/st-machine-providers-stm32mp.inc
 
 
MACHINEOVERRIDES .= ":stm32mpmydemo"
 
DEFAULTTUNE = "cortexa7thf-neon-vfpv4"
include conf/machine/include/tune-cortexa7.inc
 
STM32MP_DEVICETREE = "${CUBEMX_DTB}"
 
MACHINE_FEATURES += "splashscreen"
MACHINE_FEATURES += "watchdog"
MACHINE_FEATURES += "wifi"
MACHINE_FEATURES += "${@'gpu' if d.getVar('ACCEPT_EULA_'+d.getVar('MACHINE')) == '1' else ''}"
MACHINE_FEATURES += "m4copro"
 
DEVICE_BOARD_ENABLE_SDCARD += "${@bb.utils.contains('BOOTDEVICE_LABELS', 'sdcard', '${CUBEMX_DTB}', '', d)}"
 
FLASHLAYOUT_TYPE_LABELS_sdcard = "${@bb.utils.contains('BOOTDEVICE_LABELS', 'sdcard', '${CUBEMX_DTB}', '', d)}"
 
FLASHLAYOUT_CONFIG_LABELS_deleteall = "cubemx"
FLASHLAYOUT_TYPE_LABELS_deleteall_cubemx = "${CUBEMX_DTB}"
FLASHLAYOUT_TYPE_LABELS_extensible = "${CUBEMX_DTB}"
 
CUBEMX_DTB_PATH_TFA = "tf-a"
CUBEMX_DTB_PATH_TFA_SB = "tf-a"
CUBEMX_DTB_PATH_UBOOT = "u-boot"
CUBEMX_DTB_PATH_LINUX = "kernel"
CUBEMX_DTB_PATH_OPTEEOS = "optee-os"
 
BOOTSCHEME_LABELS += "trusted"
UBOOT_CONFIG += "basic"
 
BOOTDEVICE_LABELS += "sdcard"
 
 
MACHINE_FEATURES += "wifi"
 
#KERNEL_MODULE_AUTOLOAD += ""
 
# Set Wifi related package list needed when 'wifi' feature is enabled
WIFI_LIST += "linux-firmware-bcm43430"
 
CUBEMX_DTB = "stm32mp153c-my_stm-mx"
CUBEMX_PROJECT = "mx/MY_STM/CA7/DeviceTree/MY_STM"

But all the packages tf-a,kernel,u-boot are unable to compile.

Can anybody please help if my yocto configurations are correct or not?

Errors are ..

ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: oe_runmake failed
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: Execution of '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.6449' failed with exit code 1:
make: Entering directory '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work-shared/stm32mp1-demo/tfa-source'
Including bl32/sp_min/sp_min.mk
 HOSTCC stm32image.c
make: *** No rule to make target 'fdts/stm32mp153c-my_stm-mx.dts', needed by '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted/fdts/stm32mp153c-my_stm-mx.dtb'. Stop.
make: *** Waiting for unfinished jobs....
 HOSTLD stm32image
 
Built stm32image successfully
 
make: Leaving directory '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work-shared/stm32mp1-demo/tfa-source'
WARNING: exit code 1 from a shell command.
 
ERROR: Logfile of failure stored in: /home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.6449
Log data follows:
| DEBUG: Executing python function tfaconfig_env
| DEBUG: Python function tfaconfig_env finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C /home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp153c-my_stm-mx.dtb BUILD_PLAT=/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
| make: Entering directory '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work-shared/stm32mp1-demo/tfa-source'
| Including bl32/sp_min/sp_min.mk
| HOSTCC stm32image.c
| make: *** No rule to make target 'fdts/stm32mp153c-my_stm-mx.dts', needed by '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted/fdts/stm32mp153c-my_stm-mx.dtb'. Stop.
| make: *** Waiting for unfinished jobs....
| HOSTLD stm32image
| 
| Built stm32image successfully
| 
| make: Leaving directory '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work-shared/stm32mp1-demo/tfa-source'
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.6449' failed with exit code 1:
| make: Entering directory '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work-shared/stm32mp1-demo/tfa-source'
| Including bl32/sp_min/sp_min.mk
| HOSTCC stm32image.c
| make: *** No rule to make target 'fdts/stm32mp153c-my_stm-mx.dts', needed by '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted/fdts/stm32mp153c-my_stm-mx.dtb'. Stop.
| make: *** Waiting for unfinished jobs....
| HOSTLD stm32image
| 
| Built stm32image successfully
| 
| make: Leaving directory '/home/user/build-openstlinux-weston/tmp-openstlinux_weston-glibc/work-shared/stm32mp1-demo/tfa-source'
| WARNING: exit code 1 from a shell command.
| 
ERROR: Task (/home/user/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 720 tasks of which 650 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

Thanks in advance.

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
September 29, 2020

Hi @Hsn​ ,

It look like ENABLE_CUBEMX_DTB ?= "1" is missing in your machine .conf in order to tell system to get dts file in mx sub-folder. ( still expect it in tf-a source folder)

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Hsn
HsnAuthor
Associate II
September 29, 2020

Hi @Community member​ Thanks for your reply. I compiled it by adding the recipes and class from addons to my demo layer. kernel & tf-a compiled successfully but u-boot still not able to compile.

ENABLE_CUBEMX_DTB ?= "1" is now already in the cubemx-stm32mp.bbclass

The error log is quite big, pasting the tail of error here..

| arm-ostl-linux-gnueabi-ld.bfd -pie --gc-sections -Bstatic --no-dynamic-linker -Ttext 0xC0100000 -o u-boot -T u-boot.lds arch/arm/cpu/armv7/start.o --start-group arch/arm/cpu/built-in.o arch/arm/cpu/armv7/built-in.o arch/arm/lib/built-in.o arch/arm/mach-stm32mp/built-in.o board/st/common/built-in.o board/st/stm32mp1/built-in.o cmd/built-in.o common/built-in.o disk/built-in.o drivers/built-in.o drivers/dma/built-in.o drivers/gpio/built-in.o drivers/i2c/built-in.o drivers/net/built-in.o drivers/net/phy/built-in.o drivers/power/built-in.o drivers/power/battery/built-in.o drivers/power/domain/built-in.o drivers/power/fuel_gauge/built-in.o drivers/power/mfd/built-in.o drivers/power/pmic/built-in.o drivers/power/regulator/built-in.o drivers/serial/built-in.o drivers/spi/built-in.o drivers/usb/cdns3/built-in.o drivers/usb/common/built-in.o drivers/usb/dwc3/built-in.o drivers/usb/emul/built-in.o drivers/usb/eth/built-in.o drivers/usb/gadget/built-in.o drivers/usb/gadget/udc/built-in.o drivers/usb/host/built-in.o drivers/usb/musb-new/built-in.o drivers/usb/musb/built-in.o drivers/usb/phy/built-in.o drivers/usb/ulpi/built-in.o env/built-in.o fs/built-in.o lib/built-in.o net/built-in.o --end-group arch/arm/lib/eabi_compat.o arch/arm/lib/lib.a -Map u-boot.map; true
| arm-ostl-linux-gnueabi-objcopy --gap-fill=0xff -j .text -j .secure_text -j .secure_data -j .rodata -j .hash -j .data -j .got -j .got.plt -j .u_boot_list -j .rel.dyn -j .binman_sym_table -j .text_rest -j .dtb.init.rodata -j .efi_runtime -j .efi_runtime_rel -O srec u-boot u-boot.srec
| make -f /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/scripts/Makefile.build obj=dts dtbs
| arm-ostl-linux-gnueabi-objcopy --gap-fill=0xff -j .text -j .secure_text -j .secure_data -j .rodata -j .hash -j .data -j .got -j .got.plt -j .u_boot_list -j .rel.dyn -j .binman_sym_table -j .text_rest -j .dtb.init.rodata -j .efi_runtime -j .efi_runtime_rel -O binary u-boot u-boot-nodtb.bin
| arm-ostl-linux-gnueabi-objdump -t u-boot > u-boot.sym
| make -f /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/scripts/Makefile.build obj=arch/arm/dts dtbs
| mkdir -p arch/arm/dts/ ; (cat /home/user/user1/build-openstlinux_distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/dts/stm32mp153c-s4_m4-mx.dts; echo '#include "stm32mp153c-s4_m4-mx-u-boot.dtsi"') > arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.pre.tmp; arm-ostl-linux-gnueabi-gcc --sysroot=/home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/u-boot-stm32mp/2020.01-r0/recipe-sysroot -E -Wp,-MD,arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.d.pre.tmp -nostdinc -I/home/user/user1/build-lopenstlinux_distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/dts -I/home/user/user1/build-openstlinux_distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/dts/include -Iinclude -I/home/user/user1/build-openstlinux_distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/include -I/home/user/user1/build-openstlinux_distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/include -include /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/include/linux/kconfig.h -D__ASSEMBLY__ -undef -D__DTS__ -x assembler-with-cpp -o arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.dts.tmp arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.pre.tmp ; ./scripts/dtc/dtc -O dtb -o arch/arm/dts/stm32mp153c-s4_m4-mx.dtb -b 0 -i /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/dts/ -Wno-unit_address_vs_reg -Wno-simple_bus_reg -Wno-unit_address_format -Wno-pci_bridge -Wno-pci_device_bus_num -Wno-pci_device_reg -Wno-avoid_unnecessary_addr_size -Wno-alias_paths -d arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.d.dtc.tmp arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.dts.tmp ; cat arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.d.pre.tmp arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.d.dtc.tmp > arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.d ; sed -i "s:arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.pre.tmp:/home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/dts/stm32mp153c-s4_m4-mx.dts:" arch/arm/dts/.stm32mp153c-s4_m4-mx.dtb.d
| Error: /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/arch/arm/dts/stm32mp15-no-scmi.dtsi:103.1-5 Label or path dsi not found
| FATAL ERROR: Syntax error parsing input tree
| scripts/Makefile.lib:308: recipe for target 'arch/arm/dts/stm32mp153c-s4_m4-mx.dtb' failed
| make[3]: *** [arch/arm/dts/stm32mp153c-s4_m4-mx.dtb] Error 1
| /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/dts/Makefile:38: recipe for target 'arch-dtbs' failed
| make[2]: *** [arch-dtbs] Error 2
| /home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source/Makefile:1087: recipe for target 'dts/dt.dtb' failed
| make[1]: *** [dts/dt.dtb] Error 2
| make[1]: Leaving directory '/home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work/stm32mp1_demo-ostl-linux-gnueabi/u-boot-stm32mp/2020.01-r0/build/stm32mp15_basic_defconfig'
| Makefile:167: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| make: Leaving directory '/home/user/user1/build-openstlinux-distro/tmp-openstlinux_distro-glibc/work-shared/stm32mp1-demo/uboot-source'
| WARNING: exit code 1 from a shell command.
| 
ERROR: Task (/home/user/user1/layers/meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2020.01.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 753 tasks of which 745 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds
 
Summary: 1 task failed:
 /home/user/user1/layers/meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2020.01.bb:do_compile

Olivier GALLIEN
ST Technical Moderator
October 6, 2020

Hi @Hsn​ 

I noticed this error in log during u-boot compile :

"Label or path dsi not found"

Please have a look to :

https://community.st.com/s/question/0D53W00000JQ4z4SAD/stm32mp1-ecosystem-known-bugs-and-common-pitfalls

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.