Well, if you're interested in 8bit MCUs your needs would be met by more than 25 devices.
Would it be possible to be a little more specific?
DAC built-in or extern?
NVRAM: serial/parallel, RAM size?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
I would like to have 20 pin 8 bit micro controller and external two channel DAC will be fine : My sensor is i2c interface and external RAM like 24C512 and RTC DS1307 will be OK
Main difference between S103 and S903: the latter one also provides an internal reference voltage measurement
If SO20 doesn't fit your need please check the site of STM8 Microcontrollers and filter the required parameters on its left side, as you can see at the following example:
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.