Is it possible to share UART interrupt in dual-core microcontrollers in both cores?
Hi!
I'm trying to share one UART in both cores of the dual-core STM32H745. I'm using the HAL library.
I've achieved to transmit (in polling mode) from the two cores using a semaphore to manage access to the UART.
However, I can't receive using interrupt on both cores. I have manually activated the interrupt in HAL_UART_MspInit, but it still doesn't work. The CM7 core receives the data but the CM4 not.
I would like to receive data through the same UART in both cores. Is it possible to do what I am trying? Or I would have to pass the data myself from CM7 to CM4? Is it possible to do it on other peripherals like SPI?
Thanks for your help.