Question
Looking into accuracy of internal oscillator, and wondering if it is sufficient to drive USB as virtual COM port over large variance in temperatures.
I am using the STM32L476 MCU on a board that will be used on a boat with varying temperature conditions, and using the USB as a virtual COM port to send and receive data for diagnostics of the board. When configuring the clock using the MSI to drive 48MHz, will this internal oscillator be accurate to operate over a large variance of temperatures? Or will I need to use an external clock?