Skip to main content
Sarah1
Associate
September 22, 2020
Question

Serial communication parity bit.

  • September 22, 2020
  • 1 reply
  • 981 views

The data frame of BootLoader of STM32F207 : a start bit, data bits, even parity bit and a stop bit.The USART data contains a even parity to send to the BootLoader, then it replies with the correct data.

Theoretically, USART data has no parity bit, then the BootLoader will judge it as an error after receiving it.But in practice, BootLoader can reply with the correct information.Why the BootLoader can resolve data without parity bits?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
September 22, 2020

Wrong sub-forum..

The STM32 doesn't "receive" the 0x7F byte but rather uses it as a timing pattern to auto-baud. No sure why it is worth worrying about this when it is documented to expect 8E1, and works properly when used?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Sarah1
Sarah1Author
Associate
September 23, 2020

The STM32 receives "0x7F",it enters the system memory boot mode.And then,if BootLoader receives "0x00 0xFF" without parity bit,why it can works properly?

How can we send data when the sender does not support parity bit and BootLoader requires even parity?