Skip to main content
KSang.2
Visitor II
September 22, 2020
Question

[STM32H743I-EVAL2] Debug inquiry

  • September 22, 2020
  • 0 replies
  • 786 views

I am testing with STemWin demo program on STM32H743I-EVAL2.

​

Other applications program work well with the debugger on STM32H743I-EVAL2.

​

But the STemWin demo program only the debugger doesn't work.

​

What's the problem?

​

STM32CubeIDE Version: 1.4.0

​

0693W000004GeYVQA0.png

​STMicroelectronics ST-LINK GDB server. Version 5.6.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

​

Starting server with the following options:

    Persistent Mode      : Disabled

    LogFile Name        : C:\smkang\OneDrive\project\sugen\sample_board\STM32H7x3I-EVAL\work2\STemWin\SW4STM32\STemWin-STM32H743I-EVAL\Debug\st-link_gdbserver_log.txt

    Logging Level       : 31

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Enabled

    SWD Debug         : Enabled

​

Target connection mode: Attach

Hardware watchpoint supported by the target 

COM frequency = 24000 kHz

ST-LINK Firmware version : V3J7M2

Device ID: 0x450

PC: 0x12f0000

ST-LINK device status: RUN_MODE

ST-LINK detects target voltage = 3.29 V

ST-LINK device status: RUN_MODE

ST-LINK device initialization OK

Waiting for debugger connection...

Waiting for connection on port 61234...

Accepted connection on port 61234...

Debugger connected

Try halt...

ST-LINK device status: HALT_MODE

Enter STM32_AppReset() function 

NVIC_DFSR_REG = 0x00000009

NVIC_CFGFSR_REG = 0x00000000

Debugger connection lost.

Shutting down...

​

​

This topic has been closed for replies.