Skip to main content
Vlaty.1
Associate III
September 18, 2020
Question

Good morning, thank you for your help. Found a problem. When you select Production mode, boot_0 boot_2 on, the CD card is installed, the debugger does not start debugging mode. С уважением, �?лек�?андр.

  • September 18, 2020
  • 3 replies
  • 1415 views

..

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
September 21, 2020

Hi @Vlaty.1​ 

I see obvious message "target address not reachable" on top of the screenshot.

looks you try to use ethernet over usb connection with board. Need to connect USB cable on CN7.

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Vlaty.1
Vlaty.1Author
Associate III
September 22, 2020
Good morning. Thanks for the help. No I need to check eth0(cn8) I write > the ip addr add 192.168.1.4 dev eth0. Checking > ifconfig. The address is set. I > ping the static address I need. The result is the loss of all packets. How do I raise the eth0 interface? Sincerely, Alexander пн, 21 �?ент. 2020 г. в 17:34, ST Community :