Skip to main content
NJasa.1
Associate
September 18, 2020
Solved

Electrostatic discharge voltage capability of Diode STTH1602CT

  • September 18, 2020
  • 1 reply
  • 924 views

Hi,

Is STTH1602CT Diode having Electrostatic Discharge voltage capabilities? if yes then how much voltage? Because its not mention in datasheet.

Thanks

Nandish Jasani.

This topic has been closed for replies.
Best answer by Dario CUCCHI

Hello @Community member​ ,

The STTH1602CT is a standard dual diode with common cathode.

The two diodes have forward and reverse maximum voltage, as specified in the datasheet.

If you need to use a component in your system for ESD protection, I can suggest to visit the ST dedicated page here.

All the best !

1 reply

Dario CUCCHI
Dario CUCCHIBest answer
ST Employee
September 18, 2020

Hello @Community member​ ,

The STTH1602CT is a standard dual diode with common cathode.

The two diodes have forward and reverse maximum voltage, as specified in the datasheet.

If you need to use a component in your system for ESD protection, I can suggest to visit the ST dedicated page here.

All the best !