Skip to main content
Chandrashekar C
Associate III
September 16, 2020
Solved

SWV Trace/Console for STWIN-STWINK1 on STM32CubeIDE, anyone was able to set up a trace on STWIN-STWINK1? Is this possible? Please let me know

  • September 16, 2020
  • 6 replies
  • 1258 views

HI All,

I am using STWIN-STWINK1 for a predictive maintenance application, I am unable to set up SWV ITM data console and trace on STM32CubeIDE.

I tried following all the tutorials on YouTube and community, nothing works. If anyone has been able to get this through please let me know or share the configuration.

Many thanks in advance

Chandrashekar C

This topic has been closed for replies.
Best answer by Eleon BORLINI

Hi @Chandrashekar C​ ,

I'm wondering if the SWO pin, required for Serial Wire Viewer (SWV) trace, has been wired on STWINKT1 board... This is an optional pin, as declared by the ST LINK V3 user manual.

The schematic of the application board doesn't seem to include that pin... this may cause the miscommunication.

0693W000003RyxsQAC.png

-Eleon

6 replies

Eleon BORLINI
ST Employee
September 17, 2020

Hi @Chandrashekar C​ ,

adding more topics for community support.

I find the SWV comsol in Window - Short wiew - other - SWV, and then select for example the SWV Data Trace.

0693W000003Ry6yQAC.png

For a tutorial on how to set up the proper variables to be monitored, you can refer to this video.

-Eleon

Chandrashekar C
Associate III
September 17, 2020

Hi @Eleon BORLINI​,

Thanks for your kind response.

I have tried all these and I have also referred to the video you have mentioned in the previous message.

I am trying use SVW console for STWIN_PM_AWS application, instead of terminal, I wan to re-direct all the messages to SVW console.

Here is my debugger configuration

0693W000003RyZCQA0.png0693W000003RyZ2QAK.png

I did changed the puts function as following

/**
 * @brief Retargets the C library printf function to the USART.
 * @param None
 * @retval None
 */
PUTCHAR_PROTOTYPE
{
 /* Place your implementation of fputc here */
 ITM_SendChar(ch);
 return ch;
}

Just wanted to know if I need to enable any macro? or am I doing anything wrong here?

Kind Regards

Chandrashekar C

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
September 17, 2020

Hi @Chandrashekar C​ ,

I'm wondering if the SWO pin, required for Serial Wire Viewer (SWV) trace, has been wired on STWINKT1 board... This is an optional pin, as declared by the ST LINK V3 user manual.

The schematic of the application board doesn't seem to include that pin... this may cause the miscommunication.

0693W000003RyxsQAC.png

-Eleon