Question
PWM not working on TIM2 channel 1 on STM32H753XIH6
We are using PWM here to change the brightness of LCD display, but PWM is not working , as of now I don't have CRO's as I'm working remotely. Is there anything wrong in the below code??
#include "stm32h7xx.h"
void PwmGpioInitalize()
{
/* Timer GPIO Pin Enabling */
RCC->AHB4ENR |= RCC_AHB4ENR_GPIOAEN;
GPIOA->MODER |= (2<<(2*15));// PA15 - 10 Alternate Function mode;
GPIOA->PUPDR &= ~((1<<30)|(2<<30)); //PA15 - 00 NO PULL UP or PULL DOWN
GPIOA->OTYPER &= ~(1<<15); // 0 - PA15 Selected Push Pull type
GPIOA->OSPEEDR &= ~((1<<30)|(2<<30)); // PA15 - 00 Low Speed Selected
GPIOA->AFR[1] |= (1<<(4*7)); // Timer2 PWM Channel 1 selected as Alternate function1
}
void BacklightPinGpioInitalize()
{
/* Backlight GPIO Pin Enabling */
RCC->AHB4ENR |= RCC_AHB4ENR_GPIOEEN;
GPIOE->MODER |= (1<<(2*2)); //PE2 - Output Mode
GPIOE->PUPDR &= ~((1<<4)|(2<<4));// NO PULL UP or PULL DOWN
GPIOE->OTYPER &= ~(1<<2);// PE2 Selected Push Pull type
GPIOE->OSPEEDR |= (2<<(2*2)); // HighSpeed is selected
}
/** Timer_Clock = 2 x APB2_clock = 200 MHz */
/** PWM_freq = Timer_Clock /(Period x (Prescaler + 1))*/
/** PWM_freq = (200*1000000)/(40000*1) = 5000 Hz*/
void PwmTimerInit(void)
{
RCC->APB1LENR |=RCC_APB1LENR_TIM2EN; // Timer2 Clock Enable
PwmGpioInitalize(); // Initialize the PWM Channel 1 GPIO - PA15
TIM2->CCMR1 = 0X00000000; // y De initialize
TIM2->CR1 = 0x0000; // No clock division, Up counter mode,Edge Aligned mode
TIM2->PSC = 0; // Precale value TODO:Needs to fix the PWM Frequency
TIM2->ARR = 40000 ; // Set to maximum
TIM2->CCR1 = 20000 ; // 50 % duty cycle set
TIM2->CCMR1 |= (TIM_CCMR1_OC1M_1|TIM_CCMR1_OC1M_2); // y 0110 - Pwm Mode 1 is selected
TIM2->CCMR1 |= TIM_CCMR1_OC1PE; // y Preload register enabled
TIM2->CR1 |= TIM_CR1_ARPE; // Auto preload register enabled
TIM2->CR1 &= ~TIM_CR1_DIR; //ch Countermodedirup
TIM2->CCER &= ~TIM_CCER_CC1P; // Output Polarity high
TIM2->CCER |= TIM_CCER_CC1E; // Signal output enable on the pin
TIM2->CR1 |= TIM_CR1_CEN; // Timer Enable
}
void LcdSetBrightness( uint8_t BrightnessValue )
{
uint32_t Pulse;
/* Setting up pulse value for brightness */
Pulse = (uint32_t)((40000 * BrightnessValue) / 100);
/* Set the Capture Compare Register value */
TIM2->CCR1 = Pulse;
}
void LcdBacklightOn( void )
{
GPIOE->ODR |= 1<<2;
}
void LcdBacklightOff( void )
{
GPIOE->ODR &= ~(1<<2);
}
int main()
{
BacklightPinGpioInitalize();
PwmTimerInit();
LcdBacklightOn;
LcdBacklightOff;
LcdSetBrightness(60);
}