Skip to main content
RJain.2
Visitor II
September 15, 2020
Question

Getting Hardfault handler when we do the DAC init between any of the other peripheral init in the start of the main function

  • September 15, 2020
  • 0 replies
  • 687 views

Hi to All,

I like to inform you that i am using the STM32F103RC controller and the problem is that when i do the DAC init between any of the peripheral init in STM32CubeIDE inside the main function, than i am getting the hard fault handler as shown below :

int main(void)

{

 HAL_Init();

 /* Configure the system clock */

 SystemClock_Config();

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_DMA_Init();

MX_RTC_Init();

MX_DAC_Init();

MX_I2C1_Init();

MX_SPI2_Init();

MX_USART1_UART_Init();

MX_USART2_UART_Init();

while(1)

{

// application level logic

}

}

But when i define the DAC init at the last after initialising all other peripherals than i do not get the hard fault handler as shown below:

int main(void)

{

 HAL_Init();

 /* Configure the system clock */

 SystemClock_Config();

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_DMA_Init();

MX_RTC_Init();

MX_I2C1_Init();

MX_SPI2_Init();

MX_USART1_UART_Init();

MX_USART2_UART_Init();

MX_DAC_Init();

while(1)

{

// application level logic

}

}

DAC init is generated by the STM32CubeMX as shown below

/* DAC init function */

void MX_DAC_Init(void)

{

 DAC_ChannelConfTypeDef sConfig = {0};

 /** DAC Initialization

 */

 hdac.Instance = DAC;

 if (HAL_DAC_Init(&hdac) != HAL_OK)

 {

  Error_Handler();

 }

 /** DAC channel OUT1 config

 */

 sConfig.DAC_Trigger = DAC_TRIGGER_NONE;

 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;

 if (HAL_DAC_ConfigChannel(&hdac, &sConfig, DAC_CHANNEL_1) != HAL_OK)

 {

  Error_Handler();

 }

 if (HAL_DAC_Start(&hdac, DAC_CHANNEL_1) != HAL_OK)

 {

  /* Start Error */

  Error_Handler();

 }

}

So can you please let me know the reason behind this why i am getting the hard fault handler when i do the DAC init in between other peripheral init and not getting hard fault handler when i do the DAC init at the last of all other peripheral init.

Thanks and regards,

Ronak Jain

This topic has been closed for replies.